Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't reliably sense stalling using L6470 chip

Posted on October 22, 2013 at 20:37I've been quite successful at controlling the L6470 stepper driver chip from my embedded ARM processor for all features other than the sensorless stall detection feature. I'm hoping that I'm missing something and t...

GoTo(ABS_POS) error during motor running

Posted on September 03, 2014 at 09:59Hello!In my application I send GoTo(ABS_POS) commands when stepper motor is running at constant speed, when BUSY flag is high, so I'm sure that the target speed is reached. And everything is going well most of ti...

srg0016 by Associate II
  • 1280 Views
  • 2 replies
  • 0 kudos

a formula about duty cycle computation

Posted on August 03, 2014 at 06:34hello all :             I,recently?found that the formula about duty cycle  computation in the SW do not accord with that in the user manual . Sector ????TimePhA=T/8+?T+X-Z?/2 in the SW,however,Sector ????TimePhA=?T...

Input Voltage limit on VNH5050 Diag/ENA pin

Posted on August 14, 2014 at 03:20HiI'm designing a very compact quad VNH5050 12V Motor Driver board.I can optimize my design if I can pull-up the DIAG/ENA pins to 12V rather than the 5V Logic level.There is nothing else connected to these pins.  Al...

Problem about L6482H (OCD failure)

Posted on August 22, 2014 at 19:45HiI have developed about motor control by using L6482H. I follow circuit form reference circuit of L6482H Eval board (same part). Now I stuck at OCD failure. I have construct a new board follow Eval board. In Eval b...

prustya by Associate
  • 571 Views
  • 0 replies
  • 0 kudos

L6207 PWM Current Control Question

Posted on July 30, 2014 at 19:04Could someone please explain how current is controlled on the L6207 via onboard PWM Current Controller?  Additionally, AN1762 APPLICATION NOTE indicated a constant current could be obtained through a simple voltage di...

dstetson by Associate
  • 866 Views
  • 1 replies
  • 0 kudos

L6470 Stall detect issue

Posted on July 24, 2014 at 15:26Hello, I am posting this question that another user posted but there was no answer. Can anyone help?Can't reliably sense stalling using L6470 chipI've been quite successful at controlling the L6470 stepper driver chip...

msmith by Associate II
  • 1200 Views
  • 1 replies
  • 0 kudos

Problem for EVAL6482H

Posted on July 22, 2014 at 21:47I have used EVAL6482H board to drive a stepper motor with a spec as followed,Operating voltage: 2.5vRated current/ phase: 0.49ASupply voltage: 20vI set the parameter as followed   Stepper.setParam(TVAL_HOLD, 0x02);   ...

ywliao by Associate
  • 1003 Views
  • 1 replies
  • 0 kudos

Current readout circuit problem!

Posted on August 17, 2014 at 10:32Gigi or Dino:        I met a strange question, motor parameter in STM3210E+ MB495 successfully entered the closed loop control. Now I redesign custom board,      The open loop mode debugging hardware correctly, when...