Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6470 overcurrent errors

Posted on July 09, 2013 at 00:07I've gotten past all of my comms issues and seem to be able to talk to the L6470 reliably now.  However, I'm having trouble actually getting it to move.  I keep getting OCD events even when commanding moves at low acc...

bSwitching ON/OFF two devices using two BTA06 but same Line

Posted on May 24, 2018 at 09:31Dear All,I have been working on a project where I need to Switch on Two devices using Two BTA06 controlled by Digitally Opto-Triac. Line and Neutral are same for both.Attached is the schematic.I have issue that when I ...

Engg Try by Associate
  • 1052 Views
  • 0 replies
  • 0 kudos

L6227Q using Enable as PWM signal

Posted on May 04, 2018 at 19:12The L6227Q looks like just the part I want to control a small motor that will run at about 5V and no more than 300mA.  I was looking at Table 7 in the data sheet.  I think what I want is to set IN1 and IN2 to the polar...

0690X0000060AwnQAE.png

VNH7070AS Heat sinking

Posted on May 21, 2018 at 15:12Hi, I wondered if there were any other appropriate methods for heat sinking of the VNH7070AS H-bridge motor driver instead of using the PCB substrate?? I would ideally like to use a traditional metal heat sink instead ...

Triacs control

Posted on May 12, 2018 at 19:44 We used BT139X-600E triac. Opto triac MOC3052 used for triac's control.  Load is 230V, 50 Hz LED lamp, current is 30 mA. Current is not very nonlinear - it is short 'pulses' in the maximum of voltage 230 V.  The triac...

Stepper motor, 120Vdc, 6 Ampere

Posted on May 17, 2018 at 15:24I would need advice on how to make a stepper motor drive with a supply voltage of 120Vdc and a current of 6 nominal Amps.It seems to me there are only 2 ways, even if I do not know if they are feasible, they are:1) Use...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.