Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to start debugging STUSB4710AQTR based design

I built STUSB4710AQTR design basing in evaluation board. I connected it to Microsoft Surface Go tablet which support USB 3.1 PD . However I don't see any negotiation through CC lane: only tablet send 16Hz .Please advice what can be problem and how to...

SBerl by Associate
  • 860 Views
  • 1 replies
  • 0 kudos

Hi, How debug

Hi,I am using STUSB4710AQTR. I build my board basing on reference design. Now I connected it to Microsoft Surface Go tablet. According datasheet this tablet support USB3.1 PD. However I even don't see any negotiation through CC lanes: only tablet sen...

SBerl by Associate
  • 840 Views
  • 1 replies
  • 0 kudos

Viper 37LD - does not regulate

I have an ac dc converter project based on flyback (85-270AC / 12V_1.5A-15V_0.125mA) and at the output I do not have voltage regulated. The project was prepared with the help of e-Design.I was able to operate when I pressed the tip of the oscilloscop...

JunexR8 by Associate II
  • 974 Views
  • 0 replies
  • 0 kudos

Why is torque falling at low speed?

I'm running the motor in torque mode with an encoder. It works really well.The only problem I have is that something internal to the FOC software adjusts the torque down at (very) low and zero speed. I assume this is done to avoid the motor overheati...

Motor Control SDK5.2 with STM32F429ZI

I attended the excellent motor control sessions last week at the ST Developers Conference in Santa Clara, CA. At the presentation I received the Nucleo F302R8 and X-Nucleo-IHM07M1 boards which I've been experimenting with. However, I would now like...

EVAL-IPFC01V1 problems

Posted on September 22, 2017 at 11:45Hi,Does anybody has experience with the evaluation board IPFC01V1 for the PFC-Controller STNRGPF01?My Problem is that the board crashed at a experiment with no load connected to it.Does anybody have an Idea what ...

Powerstep01 goto at specific speed

Hi, I'm using the powestep IC to control a stepper motor. All is going well but I can't figure out how to move the motor from one point to another at specific speed. e.g. if I send the goto command, like goto(1000) the motor do Accel--->max_speed-->D...

PSlav by Associate
  • 686 Views
  • 0 replies
  • 1 kudos

What's happening with the LD39300PT-R voltage regulators?

Anyone knows what's happening with the productoion of the voltage regulator LD39300PT-R? I am trying to buy this component for weeks and all distributors have no stock of this part number. The factory delivery time, in every distributors is 50 weeks!...

DOuro by Associate
  • 701 Views
  • 0 replies
  • 0 kudos

LDL212 datasheet mistake

Hi,There is a datasheet on digikey page related to LDL212 product wihch shows pin1 is Output Voltage but the datasheet on ST website shows pin1 is Ground.I beleive there is a mistake on datasheet on digikey page.A picture is attached thanks.

iEVIN by Associate
  • 912 Views
  • 0 replies
  • 0 kudos