cancel
Showing results for 
Search instead for 
Did you mean: 

MOSFET for reverse current blocking with STEF01

Central SUPPORT
Senior II

STEF01 has an interesting price but requires an external power MOSFET for reverse polarity protection. I see from the datasheet that ST has performed some measurements using external FETs, so which one would you recommend?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Central SUPPORT
Senior II

When the application has a large output capacitor Cload, for example to power the protected circuit long enough for it to handle any required shutdown routines or to minimize the track inductance, it is recommended to implement the reverse current blocking MOSFET.

While we do not recommend any specific MOSFET, the main criterion for selecting the NMOS transistor is that it should be selected to operate within the range of the sourcing current and voltage of the Vg driver pin (30µA and Vout+10V, respectively).

In case a MOSFET with lower Vth is used, the voltage at Vg needs to be clamped to a suitable level with a clamping diode. Choosing a MOSFET with low RDSon ensures that the voltage drop, and thus power losses associated with the MOSFET, are low.

View solution in original post

1 REPLY 1
Central SUPPORT
Senior II

When the application has a large output capacitor Cload, for example to power the protected circuit long enough for it to handle any required shutdown routines or to minimize the track inductance, it is recommended to implement the reverse current blocking MOSFET.

While we do not recommend any specific MOSFET, the main criterion for selecting the NMOS transistor is that it should be selected to operate within the range of the sourcing current and voltage of the Vg driver pin (30µA and Vout+10V, respectively).

In case a MOSFET with lower Vth is used, the voltage at Vg needs to be clamped to a suitable level with a clamping diode. Choosing a MOSFET with low RDSon ensures that the voltage drop, and thus power losses associated with the MOSFET, are low.