Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

the vn808 device has a wrong datasheet which has a conflict with the app. note (AN2208) regarding to Vin rated voltage, although what should i do with the not connected pins ?

i'm working on a project uses this device (VN808_attached exact photo of the device i have) and in the datasheets carries a name of (VN808CM-32-E) i found in the absolute maximum rating table that Vin max is 5V (attached photo) in the other-hand i fo...

Ksaad.1 by Associate
  • 1458 Views
  • 1 replies
  • 1 kudos

STC3115 SOC

Hello,I am using a lithium battery to power my PCB and a stc3115 to have the state of charge. Behind the battery is a LDO to convert the battery voltage to 3.3V, so the voltage of the battery varies between 4.2V and 3.3V. I would like to change the s...

emil28 by Senior
  • 619 Views
  • 0 replies
  • 0 kudos

VNQ5050K- E Surge Issue - (what's wrong?)

Dear Community,I'm facing a bad issue on a recent board I designed.The board is supplyed by 12/24V battery and drive some magnetic valves.Unfortunately during precompliance surge test, based on EN 61000-4-5, the VNQ5050K got destroyed and the microco...

LAGOS.1 by Associate
  • 735 Views
  • 0 replies
  • 0 kudos

STC3100 Reading Current

Hi,I will use STC3100 IC at my circuit. I will use Li-ION AA type Cell in my circuit and I charge my cell externally on charge device. So ı don't use STC3100 while charge status monitoring. I will use STC3100 only monitoring available charge status. ...

KOKŞA.1 by Associate
  • 715 Views
  • 0 replies
  • 0 kudos

Phase current isn't precise at different speed

Hi all,I am using STM32F303RE + IHM08M1 to do a bike project (250W/36V motor).When the motor ramp up, I found the current will output very low and become higher according to speed.I connected a current meter between battery and the board, I found the...

JHsu.13 by Associate
  • 802 Views
  • 0 replies
  • 0 kudos

spice models for ST1L05CPU33R

Hi , We are using ST1L05CPU33R in our Design. We need spice models for ST1L05CPU33R. If you have this. Could you Please share with us.Thanks & ReagrdsKranthi

KRach.1 by Associate
  • 711 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.