Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Increase range between STEVAL-ISB045V1 and STEVAL-ISB68WAM

Not sure if this is the right section to ask this, but I can't find a section specifically for wireless power transfer.I am using the STEVAL-ISB045V1 and STEVAL-ISB68WAM QI wireless power eval boards. Looking at the general capabilities of QI, it can...

AClif by Associate III
  • 796 Views
  • 0 replies
  • 0 kudos

How to enable two seperate Rails with the STUSB4500L

We have an application we would like to power via USB PD. The device needs 12V or more to fully operate. To do a firmware upgrade 5V is sufficient. But the 5V are on a different Rail, normally supplied from the 12V Rail via DCDC converter. So we need...

Rico Rico by Associate II
  • 1786 Views
  • 1 replies
  • 0 kudos

Questions about transformer design of VIPER265KDTR

Input: Single-phase AC70-500VOutput: DC24V5WOutput diode voltage drop: 1.25V1�?My design idea is this, design the transformer to work in CCM mode (current ripple coefficient 0.85) at the lowest input voltage and full load, and enter DCM mode after th...

Resolved! Cannot install firmware or drivers for STEVAL-PCC009V2 board to use eval6470pd board due to Windows error

When I run the updater, and press 'start', an error occurs during the step, "Install IBUUI drivers". The error message isError installing C:\Program Files(x86)\STMicroelectronics\SPINFamily Evaluation Tool 3.2\Updater\Drivers\WinXP\IBUUI.inf driver. ...

ENovk.1 by Associate II
  • 1319 Views
  • 1 replies
  • 0 kudos

48V BLDC motor controller for EV application

hi, i am working for finding BLDC motor control evaluation board for my EV application.from ST -- > found STEVAL-SPIN3202 from the website. i would like to know the details of the STEVAL-SPIN3202 -- max peak current withstanding capability and any de...

Jana by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

i need to charge 18650 li ion battery using SPV 1050 MPPT IC. where will i need to connect the load (microcontroller)? on which pin do i need to connect my micro controller?

Do i need to connect my load on STORE pin or in parallel to VBATT+ ?In STEVAL-ISV020V1 what is EXT_SUP? is this where i need to connect my loadwhat will happen if i discharge 1 Amp current from 18650 battery?what is the current capacity of inbuilt P...

TVard.1 by Associate III
  • 715 Views
  • 0 replies
  • 0 kudos

Hi, IC L6564 O/p voltage 24VDC is fluctuating .

HI, We are using IC L6564 for application of AC to DC power supply 24VDC/1.5A . But We are getting fluctuating output vltg in between 20V to 24V without load .When 1k load is connected then output drop down & we get 13Vto 15V.

L9963 BMS IC Programming Document and other informations

Hi ST,I am interested In using the L9963 IC for UPS battery management system.Since it is a UPS, i am not intending to use the default SPC574S64E3 but another STM32 MCU.The following are my questions:Is there any Programming Manual for the L9963 IC a...

GLasw.1 by Associate II
  • 945 Views
  • 0 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.