Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi,in my project i have a requirement for a startup time of one second, how can i ajust that parameter?Thanks for helping
In the datasheet it says there are Type A, C and E for DPAK. How will i know which is the correct type of DPAK for this part number? STD2HNK60Z
we want to develope simple BLDC driver in open loop mode with speed and direction control input.I found your IC L6235 which fits to our requirement .is there any evaluation kit this IC.
Hello, I've plugged a dremel on 220V and the TRIAC on it blew up, the code is: Z0MF713 I'm having trouble finding it to fix my equipment, any clues?
The circuit is intended to recharge a NiMH battery, with a input voltage (Vin) of 15V.Using Rsense in series with the inductance I have a maximum output voltage (Vout) of Vin - 1.5V.If instead Rsense refers to GND, I can reach 100% dc.This behavior p...
Hi, I cannot find in the datasheet whether the base of the STBR6012 is electrically isolated, and if so what the isolation voltage is.Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.