Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dear all, I am trying to use STPM33 to measure Voltage.I refer to "STSW-STPM002" reference design. We read with interval: 5s. The reading value is repeated: value-value-0000-value-value-0000......I don't know why there is 0000. Can you help me?

Set up > Config: default (reg0 ~ reg19) > Latch: by SYN and SCS pin > Interface: uart > Reading interval: 5sLogCall emberAfPluginPowerMeterIcReadEventHandleruUART0_SSB_TX_Buffer[0]:48uUART0_SSB_TX_Buffer[1]:FFuUART0_SSB_TX_Buffer[2]:00uUART0_SSB_TX_B...

NCao .1 by Associate
  • 727 Views
  • 0 replies
  • 0 kudos

Please decipher the release date (year and week), assembly location and wafer lot (LD1117DT18TR PBF)?

Я хотел бы получить дополнительную информацию о маркировке LD1117DT18TR PBF:ST (e3) GN L1117      18GKOW7347ST - �?то логотип производител�? STMicroelectronics. Явл�?ет�?�? ли LD1117DT18TR PBF оригинальным продуктом вашей компании? Пожалуй�?та, ра�?ш...

PMolc.1 by Associate
  • 873 Views
  • 0 replies
  • 0 kudos

Explanation of Pil simulation times in Simulink

Hello, i'm here to ask you becouse i not understand how improve (if possible) the time spees in PiL mode. i've build my FOC+Space Vector compute model on simulink (there are sin, cos functions for Park Transforms ) with fixed step size of 1us, and 1....

0693W000001roTcQAI.png

Aktive Freewheeling

Hello,has the VNH7070AS an active freewheeling mode implemented?best regards

ISchu.1 by Associate
  • 866 Views
  • 0 replies
  • 0 kudos

I have a custom PCB with a STM32L476RG MCU and I would like to use it to communicate with the EVALSTPM32 power meter. But how do I connect the two together?

As shown in my picture, I have connected both 3.3v to both the board and the uart pins and veried that it is providing 3.3v. Is this the correct connection? Should I be expecting something from the uart pins? I haven't done any configurations yet.

0693W000001rsbVQAQ.jpg
SWong.2 by Associate
  • 752 Views
  • 0 replies
  • 0 kudos

STEVAL-GLA001V1 capacity

How much is the max load current capacity for every load output of the STEVAL-GLA001V1 evaluation board?Thank you

VDuch.11 by Associate II
  • 758 Views
  • 0 replies
  • 0 kudos

What are the "STM32-based control board"?

In the manual of STEVAL-IPM08B I read:"The STEVAL-IPM08B is compatible with ST's STM32-based control board, enabling designers to build a complete platform for motor control."I wonder what are these "STM32-based control board" that are compatible wit...

Mark81 by Associate III
  • 2250 Views
  • 4 replies
  • 0 kudos

STM-PLC bug9

URL: https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-ind-plcwifi1.htmlType:  Buffer overflowDescription: Within the while loop as shown in line 536 of Lad...

SDawn.1 by Associate II
  • 839 Views
  • 0 replies
  • 0 kudos

STM-PLC bug8

URL: https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-ind-plcwifi1.htmlType:  Buffer overflowDescription: The variable component_index is used as an index ...

SDawn.1 by Associate II
  • 816 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.