Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need help setting up STEVAL-3DP001V1

Hello,I got this board and connected power and could not see any activity on the ST-LINK USB port (J11). I installed the drivers and used 115200,8,N,1, no flow control. There's no startup message or response to CR or serial echo.I can connect to the ...

Jim1 by Associate II
  • 3323 Views
  • 6 replies
  • 1 kudos

LDLN025 stop behaving as expected.

Hi!The company I work for have a product that uses the LDLN025 LDO regulator. The LDO drives an SIGFOX module, a couple of pullup resistors that goes to a always-powered uC and to a ST25DV64K IC. All of them has 100nF decoupling capacitors + a 22uF o...

FERD20L60C, Using this product in a simple 3ph rectifier and find that the diodes show conduction in both directions using a commercial quality DMM, but only in one direction using a higher quality meter, why?

FERD20L60C, Using this product in a simple 3ph rectifier and find that the diodes show conduction in both directions using a commercial quality DMM, Behave as one would expect using a higher quality meter, why?Using two inexpensive, but not junk DMM...

ANels.2 by Associate
  • 811 Views
  • 1 replies
  • 0 kudos

How do I add the X-NUCLEO-IHM05A1 drivers to a new project?

I have been able to compile and load the X-CUBE-SPN5 example to my NUCLEO-F401 with an IHM05A1 board. I notice in the example folders that there is a BSP folder with L6208 component and MotorControl folders. How can I make these folders/drivers acces...

JWhit.3 by Associate II
  • 736 Views
  • 0 replies
  • 0 kudos