Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm using SPV1050 for charging with 18650 batt with 12V Voc panel 280mA, 2.8W.. Would want to know whats the max. input current the IC can withstand..

I'm using SPV1050 for charging with 18650 batt with 12V Voc panel 280mA, 2.8W.. Would want to know whats the max. input current the IC can withstand.. Config settings are R1-10M, R2-1M, R3-5.6M & R4-6.2M, R5-500K, R6-2.7M.. Output current is limiti...

AK H by Associate II
  • 650 Views
  • 0 replies
  • 0 kudos

SPV1050 very bad efficiency with solar panel. In same condition charge current is 15mA with spv1050 and 50mA with battery directly connect to solar panel. Help need

I use a solar panel ref SM141k08l from IXOLAR and the sp1050 schematic from eval board ISV020V1 in a buck boost version. Just change some resistor to adjust Vppm to 4.8v (I got it in my test, but only 15mA is push to my Lipo battery, lipo voltage is ...

Efian.1 by Associate II
  • 1642 Views
  • 2 replies
  • 0 kudos

STNS01PUR LDO spike during 5V connect

I am seeing pretty poor performance from the LDO on the STNS01PUR when 5V is attached to the charging chip. When 5V is applied there is an initial moderate spike in the LDO output, followed by a much bigger and prolonged spike after several ms. The...

0693W0000059FqAQAU.png 0693W0000059FqFQAU.png
AKrej.1 by Associate
  • 906 Views
  • 1 replies
  • 0 kudos

non-isolated AC-DC Converter limit inrush current

Hello,I tried to design a Buck with Viper. But now I have some problems selecting the right Components. Can sombeody help me finding right Component for Rin? (13Ohm)? How much power have Rin to dissipate? Can also somebody help me in estimating inrus...

CTuts.1 by Associate
  • 747 Views
  • 0 replies
  • 0 kudos

Where can i find a Power Delivery source/sender

I have to create a wall plug from a dcdc net 48v input to 5,12 and 20v output. I have to charge multple things at these voltages via Usb-C. The consumers already have PD in their system so they can ask the voltage needed.But i can't find a power deli...

MLeen.2 by Associate
  • 946 Views
  • 1 replies
  • 0 kudos