Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LM317 adjustable voltage setting question

I'm reviewing the datasheet for the LM317 linear regulator, and it lists the equation for calculating voltage as:VO = VREF (1 + R2/R1) + IADJ R2If I plug in the numbers from my circuit (and neglect the error calculation), I get:1.25 * (1+(1400/400)) ...

gdecker1 by Associate II
  • 495 Views
  • 1 replies
  • 0 kudos

L6566bh Flyback Startup failure

I have followed the design attached in PDF. It is from ST designsuit.I have used MYRRA 75032 flyback transformer. (Datasheet Attached)Optocoupler 140105146000 with CTRmin - 50%, CTRmax - 150%.So now problem is I am not able to get continuous Vout fro...

Rajesh_J_4-1759908394615.jpeg Rajesh_J_5-1759908530633.jpeg Rajesh_J_0-1759908046874.jpeg Rajesh_J_6-1759909916995.jpeg
Rajesh_J by Associate
  • 369 Views
  • 0 replies
  • 0 kudos

Resolved! Demo Code of AEK POW BMSLV

Hi, I wanted to ask the group if the demo code "SPC58EC - AEK_POW_BMSLV application for discovery" already includes automatic cell balancing, or if it doesn't, or if it needs to be enabled somehow. I was also interested in knowing if there was a GUI ...

antonio0101_0-1759412267073.png

Resolved! STSW-WBC2STUDIO

   Hello STMicroelectronics Support Team, I would like to make a custom wireless power transfer based project. I was trying to download the GUI (STSW-WBC2STUDIO). I am planning to use STEVAL-WLC38RX and the STEVAL-WBC2TX50. Please send me the softwar...

G1 by Associate
  • 2260 Views
  • 1 replies
  • 0 kudos

Resolved! powerSTEP01 motor current unstable in one direction

I have a powerSTEP01 driving a stepper motor with the coil current set to 2A. However, the current flowing in the coils is unstable when it is flowing in one direction:Sorry about the image quality - I have an old 'scope, so had to use a photo ;)The ...

IMG_2335.jpeg
CTapp.1 by Senior III
  • 700 Views
  • 1 replies
  • 0 kudos

Resolved! STWLC38 not working

Hi! We have designed a custom board using STWLC38 but its not working. We also have the Evaluation kit of STWLC38 and Im using the same coil to test my custom board. Im getting roughly 0.6V at VRECT pins after nearly every second.  I aslo have attach...

Resolved! AEK-POW-BMS63EN reset state

Hi,I am working with a battery pack and the BMS. I have connected everything correctly to the board and after a first run everything seemed to work properly, the board was receiving commands from the MCU through the translator ISOSPI, and the green l...

M47 by Associate II
  • 706 Views
  • 3 replies
  • 0 kudos