Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PM8803C asserts TP2 without 802.3at Type 2 sequence

I have a PM8803C which asserts the TP2 pin when it only sees a single classification event (vs 2 event for Type 2 per 802.3at standard). I believe a non-standard 2.3ms 6v pulses for 114ms delivered on power up triggers the PM8803C to assert TP2.Can a...

AChas.2 by Associate
  • 815 Views
  • 0 replies
  • 0 kudos

Resolved! HI, I'm testing STEVAL-ISA178V1 evaluation board. When I connect the DC output to the oscilloscope, it gets short circuited.

The fuse of the AC mains gets switched off. I tried to connect the oscilloscope through a 10k resistor and the same behavior was observed. However, I could verify that the switching regulator works fine by measuring the voltage with a voltmeter. Both...

TAswi.1 by Associate
  • 1926 Views
  • 3 replies
  • 0 kudos