Hi, I have 50Hz sinewave with 660mVp-pk, should i connect this to SDADC analog input? It can measure negative cycle of the sinewave? i.e. If i configure SDADC as single ended zero reference mode then it can measure negative cycle of the sinewave?Na...
Hi, I am looking AC Induction motor evaluation kit. I have worked experience with STM32F4 and STM32F7 series microcontroller. So i need to make AC Driver for AC Induction Motor with all Four Quadrant operation. So please suggest me the AC Inductio...
Hi, I use STM32CubeIDE and I use STM32CubeMX configuration tool. Selected device is STM32F407VGTx. As per datasheet HCLK Max frequency is 168MHz for mentioned device. But STM32CubeMX Clock configuration tool is allowed to set frequency which is m...
Hi, I am using ST Visual Develop environment for programming of STM8S207, i am using 4.3.6 version. Problem is, whenever i give save command, STVD is halt and shown "Not Responding" My laptop configuration is Pentium Dual Core, 2.0GB RAM, Window ...
Hi, How can i define global variable in COSMIC C Compiler for STM8S? Is there any document which can explain for global variable definition in COSMIC C Compiler?Regards,Nandish Jasani.
Thanks Philipp for your reply, Actually i have main.h file where i define some constants and function declarations. I include this file in my main.c program. But in main.h file when i define constant array variable, compiler gives the error. Below ...