Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! X-NUCLEO-IHM07M1 can not drive l6230 through input PWM to obtain normal and stable voltage due to overcurrent protection

Hello,I have a X-NUCLEO-IHM07M1 suite. When I used this hardware and the FOC algorithm(PWM frequency is 8kHz) to drive a BLDC motor. Then I found that the overcurrent protection was always triggered, but I didn't know why it was triggered and how to ...

0693W00000UoauZQAR.jpg 0693W00000UoaueQAB.jpg 0693W00000UoaujQAB.jpg
Neal by Associate
  • 1576 Views
  • 1 replies
  • 0 kudos

USB-C PD Controller STUSB1702 : SRC / DFP Role

Hello,I would like to use an stusb1702 on my custom board as source / DFP docking. I found git project for an stusb1602 and nothing for stusb1702. Can someone confirme to me that I2C Register Map is the same between both. Indeed I am not able to writ...

PPaul.3 by Associate
  • 956 Views
  • 1 replies
  • 1 kudos

I want to use STEF01 as efuse in my circuit. I have a fairly big capacitance at the output of this chip, which is around 4mF.

 I am planning to turn on the chip really slow, around 0.5s, so the current going through the internal MOSFET is going to be small. The input voltage is about 24V, i do not plan to use external MOSFET. so the issue is, I do not see SOA of the intern...

GZhan.7 by Associate
  • 817 Views
  • 0 replies
  • 0 kudos