Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6389E spice model

I design a pulse output circuit using the L6389E. I'm looking for the L6389E spice model, where can I find it? Thanking you in advance.

STPM34 using SPI with multiple devices on bus

I'm experiencing issues when I talk to other devices on the SPI bus and then talk to the STPM34.I've confirmed the startup sequence of the STPM34 is correct, and if I never talk to the other device(s) there is no issue with the STPM responses.However...

Resolved! How to use STEVAL-IPMM10B for voltages lower than 125 VDC?

Hi. I am interested in using the STEVAL-IPMM10B evaluation board to drive a BLDC motor with the voltage rating of 50 V. The evaluation board user manual says, it works for 125-400 VDC. Is there any way I can use this board for lower voltages? Thanks.

AShag.1 by Associate
  • 2276 Views
  • 3 replies
  • 0 kudos

STWLC68 PROBLEMS

Hi all,We're on a project which involves WPT, so we selected the STWLC68 component. We bought the evaluation board STEVAL-ISB68WA and we tested it with the steval-isb045v1 base, as indicated. Once verified the functionality and the tuning procedure, ...

ALeon.11 by Associate
  • 1086 Views
  • 2 replies
  • 0 kudos

L7987LTR marking

Dear Support,Please advise if the DC is shown in the topside marking of part number L7987LTR?Kindly advise how to read DC. Thanks

igamoso by Associate III
  • 748 Views
  • 1 replies
  • 0 kudos