VN750PTTR-E Date Code
Dear Support,Please confirm if the DC for the part number VN750PTTR-E in the marking "235" is 2235.Year: 2022 and Week 35.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Dear Support,Please confirm if the DC for the part number VN750PTTR-E in the marking "235" is 2235.Year: 2022 and Week 35.
having errors that i cant get rid of is there an update on that one or a tuturial on how to work with that PLC?
Hi,We are using STM6904TWEDS6F. But we are confused with the open-drain status of the RST pin. The pin description states RST is open drain output. But in the AC/DC parameter list of the datasheet specifies the RST w.r.t. VCC. Is it necessary to conn...
Hello,We are facing a problem with the use of Viper16LD.My schemtic is like following: We already produce over 100 board without problem.Now, on a new batch, we have a problem.The input vlotage named "DCBus" start at 220*1.41 = 325V.With that, Viper ...
Hi ST experts,Would like to check if we are doing the testing of thermal rise on the STGIPQ8C60T, what will be the maximum temperature of the device can be sustained? Does it refer to the Tc in the datasheet~ 100degC?What is the pin of the device for...
I've certainly a problem with the RC OFF and RC Pulse definition....On RC pulse: 82k / 22nFOn RC OFF: 91k/470pFDo you have an idea to solve my problem??? Thanks for your help.