Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where is 3.3V or 5V coming from?

I have a STEVAL-IPM05F. My goal is to switch on/off the IGBTs. While I try that, I got many difficulties, like loading the Boots voltage etc. Now I have four questions. Why are all of the bootstrap capacitors carched although I don't switch the LOW-S...

IGücl.1 by Associate II
  • 4912 Views
  • 8 replies
  • 0 kudos

Resolved! L297/1 authenticity and poor process finishing

we have bought a batch of L297/1, and found the appearance has shown very bad surface plating result. we have bulk ID on the outer box, please help to confirm if the parts are authentic from STM.[edit: some information removed by moderator] thank you...

LWU.31 by Associate II
  • 2875 Views
  • 4 replies
  • 0 kudos

STNS01 question

1/At present, the most important problem is that after activating IN (input effective power supply), turning off SD (high level), and operating for many times, LDO has voltage output when IN is activated and has input all the time. Once IN has no inp...

LYUNZ.1 by Associate
  • 760 Views
  • 0 replies
  • 0 kudos

B-G431B-ESC1 - Encoder Connection Problem

Hi everyone,I recently purchased the B-G431B-ESC1 kit. I did a sensorless experiment with the ST motor control workbanch and it worked as expected. However, when I want to test with the encoder, the rotor remains locked and does not rotate after alig...

mckmk by Associate II
  • 4113 Views
  • 9 replies
  • 0 kudos

Bootstrap Capacitor value STDRIVEG600

Im not sure how to figure out the value of the bootstrap cap. Because I want to drive mosfet with 400kHz (I want to use it in a audio application) and the bootstrap diode is rated with typically 140ohm in datasheet. Problem: I see the mosfet charge i...

256QAM by Associate
  • 1184 Views
  • 1 replies
  • 0 kudos

L9963E supply

Hi,I am designing a BMS exploiting the L9963E ic. The battery pack is a 144V one, made of several lipo cells in series. I'm going for a Distributed configuration, using a master board and 3 slave PCBs. The question is:The VBAT pin cannot support volt...

SBas3 by Associate II
  • 1717 Views
  • 0 replies
  • 0 kudos