cancel
Showing results for 
Search instead for 
Did you mean: 

I am using LNBH26. I want to use the 22kHz tone amplitude as 400mV, but is there any function to change the amplitude?

HMyeo.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @HMyeo.1​, to the community!

no, the amplitude of the 22kHz tone generator cannot be changed in the LNBH26.

There is even an internal diagnostic function (see data sheet, section 2.12) that can be used to monitor both frequency and amplitude of the 22kHz tone for compliance with the limits in table 19. An internal change of the amplitude would lead this monitoring ad absurdum.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.