Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Marking smd

Hello, please help, I can’t identify the SMD component and its datashit, ST G AC GP 752.

0693W00000WLacLQAT.jpg
AutoLab by Associate
  • 1919 Views
  • 2 replies
  • 0 kudos

On Application Note AN5114 Controlling a Triac with a phototriac, at page 6/27, Section 2.4, it is mentioned that adding RGK is to reduce spurious triggering of power Triac at high temperature. Is there a chart plotting chance of occurrence vs temperature

Full note below:"At last, a resistor RGK between gate and A1 (this terminal is still also called “cathode�? as a reference to a Triacformed by two SCR) finalizes the drive circuit. Its purpose is to reduce spurious triggering of the power Triaccaused...

SXAw by Associate
  • 1490 Views
  • 0 replies
  • 0 kudos

STEVAL-DPSLLCK1 code

I have to buy three STEVAL-DPSLLCK1 in order to make three Dual Active Bridge bidirectional DC-DC converter prototypes.I need to add some functions to its fw. It is the source code available.RegardsPaiardi Giuseppe

GPaia.1 by Associate
  • 1430 Views
  • 1 replies
  • 0 kudos

VN5T006ASPTR-E Date Code

Please help to share any docs showing date code in the top marking for the part number VN5T006ASPTR-E. The marking "209" denotes DC 2209 whist marking 101 denotes DC 2101. Please refer to attached photo for reference. Thank

igamoso by Associate III
  • 3405 Views
  • 3 replies
  • 0 kudos