Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I specifically need info on how Rdson is impacted when the Vbat pin is set to a lower voltage than the battery / DRN connection. My aim is to use the L9733 in a 24V vehicle application.
Hi all, I am using the ST EVALKIT-ROBOT-1 with the latest firmware STSW-ROBOT-1.Currently, I am facing issues in establishing a serial communication with USART1 (based on interrupt), through which I can control the position of the motor.How should my...
I've selected L99LD21 LED driver for my application. I need SPI register map for configuring the device. Could anybody support me please.
Hi,I am evaluating STEVAL-ISA172V2 evaluation board and am going to develop 2KW D-SMPS , for that am unable to find firmware code and firmware user guide documents. Please provide necessary information for the above D-SMPS.
In datasheet there is no any connection between VSA and/or VDD. In block schematic are these two voltages separated, also any mention about VSA voltage required to SPI function...