Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resonant Inverter, 100 kHz, 100W. L6565 ?

I need to make a Resonant Inverter, with AC output.Application is an AC power supplyTopology: LLC or otherInput: 12V to 24V DCNo DC output100 kHz100W0 to 20A continuousconstant voltage0 to 5VInductive load for galvanic isolationpure sinesoft-switched...

The BOOM by Associate III
  • 940 Views
  • 0 replies
  • 0 kudos

Why Minimum 125V DC Supply Voltage for STEVAL- IHM023V3 ?

I have been using the PWD13F60 dual H Bridge IC which is a great device but the EVALPWD13F60 Eval board is limited to 2A_rms even though the IC is good for 8A DC due to thermal limitations of the eval board which is a shame as I really need to get a...