Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADコン�?ータ―�?�電�?VDDA�?�ノイズ�?��?�る�?�変�?�データ�?�ノイズ�?��?��?�れる VDD�?�別�?�ノイズ�?�少�?��?�電�?�?�VDDA�?�供給�?��?��?�。ADC�?�高PSRR�?��?��?��?��?

VDD�?��?�電�?�?�ノイズ�?��?�り�?�??れを使用�?��?�ADC�?�VDDA�?�ノイズを供給�?�る�?��?変�?��?�れ�?�データ�?�ノイズ�?�混入�?��?��?�。VDDA�?�ノイズフリー電�?を供給�?��?��?�。VDDA�?�VDD�?��?��?�電�?を使用�?�る必�?�?��?�る�?��?��?��?�を教�?��?��??�?��?��?�。Eng: If there is noise in the power supply to ...

andykh by Associate
  • 1439 Views
  • 1 replies
  • 0 kudos

X-NUCLEO-IHM03A1 max voltage

Why is the input voltage of the X-NUCLEO-IHM03A1 dev board limited to 50V? Looking at the schematic and BOM I don't see any reason why it shouldn't be 85V. This question has been asked before but didn't receive a clear answer.

Ben S by Associate II
  • 1132 Views
  • 1 replies
  • 0 kudos

TSCA and CP65 certificate

Dear team, can you check whehter TSCA and CP65 certificate available for MPN STMPS2161STR AND TL084IDT? thank youTSCA:Toxic Substances Control ActCP65: California Proposition 65

VHuan.3 by Associate
  • 1571 Views
  • 0 replies
  • 0 kudos

L9963E does not work in direct SPI mode (SPIEN = 1)

I am using EVAL-9963EFrom datasheet, when SPIEN pin of L9963E is connected to VCOM and R43, R46, R57, R138, R139, R140, R141, R143 are assembled, L9963E is now ready to use direct SPI (normal SPI without isolation). 1 MCU communicates with 1 L9963E o...

PHoan.2 by Associate
  • 1214 Views
  • 0 replies
  • 0 kudos