User Activity

What's the least expensive device that can receive analog audio in, and output I2S audio data?Input resolution should be 16 bits or higher, sample rate 48 kHz or higher. Is there a dedicated ADC chip? or, the STM32G030?
I need to make a Resonant Inverter, with AC output.Application is an AC power supplyTopology: LLC or otherInput: 12V to 24V DCNo DC output100 kHz100W0 to 20A continuousconstant voltage0 to 5VInductive load for galvanic isolationpure sinesoft-switched...
I need a 100 kHz, sinusoidal AC constant-voltage power supply, feeding an inductive load. Can i make a power inverter designed like a class D audio amplifier.  Except, instead of a speaker, it's a hungry power load that wants up to 20A, 5V AC power. ...
Is it possible to update executable code without reflashing the entire device, and without overwriting the entire codebase?Ie,multiple applications, such that individual applications can be separately installed, updated, and uninstalled?We don’t want...
One user mentions noise from USBhttps://community.st.com/s/question/0D50X00009XkfMDSAZ/stm32f4-adc-noise-with-increased-activity-in-usb-fsOther comments:Keep the wiring short, and make sure the resistor value matches the ADC input impedance. I’ve suc...
Kudos from