Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

e Design studio

Dear Sir,   I am not being able to complete SMPS my design using e Design Studio.design is not moving forward after filling all the parameters in properly ,  Kindly help by giving proper solutionThanking you sir 

Raju0901 by Associate
  • 1081 Views
  • 1 replies
  • 0 kudos

Driving both channels parallel on vnd products

We have multiple VND5160AJ-E on a new product were we use every single channel as an output channel. Some outputs should driver 4 Ampere which would be perfect doable if we run both channels in a chip parallel. So are the any concerns about doing thi...

rkager by Associate II
  • 876 Views
  • 0 replies
  • 0 kudos

LED2001 no output

Dear Support and Expert, We are using LED2001 to drive a LED, 2V@4A. the 6 boards come back. 4 work good but 2 no output voltage. we are using QFPN package, is there a way to check the pins are properly soldered beside take it out and reinstall? 2. i...

Dsun.21 by Associate II
  • 2824 Views
  • 2 replies
  • 0 kudos

SPV1050 Input/Output Power Tuning

Hi,I’m prototyping with the SPV1050 Eval board (the buck-boost) version and I’m facing the following issue:I had to disable the MPPT since my power source is not a solar panel. It’s a generator (AC) being rectified into a DC voltage. But that’ll come...

Tulkas by Associate
  • 1627 Views
  • 1 replies
  • 0 kudos

Resolved! please reply my question regarding L9369

Hello ST team. i wrote about L9369's AD measurement before, but i can't get any response from ST team.(my question is : https://community.st.com/t5/interface-and-connectivity-ics/l9369-getting-voltage-from-sh1-sh2/td-p/589290)i also can't find any me...

ldong.1 by Associate III
  • 2156 Views
  • 3 replies
  • 1 kudos

STUSB1602 2 port source at the same time

Hello,I am trying to negotiate set the 2 ports as a source at the same time using the firmware package "STSW_STUSB012_v1_1". When I work only 1 port it is succesfull to be source which has the profiles (5V-3A, 9V-3A, 15V-3A, 20V-5A) and it negotiates...

Enquiry for MOSFET

Hello,We are looking for top cooled Mosfets of rating ID around 40 to 60A and Vds 650 to 750V. kindly let me know if any parts are available.RegardsAnoop kumarsenior engg. Tata Elxsi Ltd.

anoopkn by Associate
  • 1074 Views
  • 1 replies
  • 0 kudos

STEF12H60M

Hello.I'm using several STEF12H60M efuses on a controll board.The setup:The CLREF resistor is 20k, the CS resistor is 3.3k and the SS cap is 100nF. This puts the efuse triping on 6.1A.I'm controlling the efuse by pulling down the on/pd pin with a npn...

licinioalmeida_0-1694688855455.png licinioalmeida_1-1694688917657.png

M4Z32-BR00SH1 MSDS

Hello.I have a bloated M4Z32-BR00SH1 battery which causes my SRAM not to retain any data. Does anyone know where can I get its Material Safety Data Sheet (MSDS)? Or may be at least an official documentation stating why it does not need an MSDS. Appar...

emaron by Associate
  • 777 Views
  • 0 replies
  • 0 kudos

Why stdriveg600 high side driver loses pulses? Can someone help me?

The circuit diagram is as follows,C1 is 0.1uf,VCC is 6V。I have the following problem:with a 100khz pwm signal (Dead Time=300ns) and with a power supply around 50v, When the current frequency is 100hz, the high side driver of the ic stdriveg600 starts...

E_G]]E4LSTIMDI38$BRQAWR.png TVIJ{8L)X1V]]6{LA{EU40B.png {3Y[{P}NCJODQ9}6}_6SL_8.png )O8`6L7RA7Z1CV`B2E@2{I5.png
likh by Associate II
  • 2379 Views
  • 5 replies
  • 0 kudos