Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Heating on VIPER22ADIP-E

Hi STMicroelectronics team,I am using VIPER22ADIP-E to design 15V, 5W power supply with input supply of 230Vac with diode bridge rectifier.The schematics file is attached here,When i am loading it with 5W load, the IC  VIPER22ADIP-E is get heated and...

Pemendra by Associate II
  • 2790 Views
  • 3 replies
  • 0 kudos

SPV1050 -- best way to switch input power between low impedance source (USB) and high impedance sources (Solar, RF, TEG)

In my application I want to be able to charge a low mAh battery using the SPV1050's built in battery charging functionality (in buck/boost mode), but I want the ability to switch the energy input from a high impedance source (such as Solar), over to ...

PMcDo.1 by Associate II
  • 3992 Views
  • 2 replies
  • 0 kudos

STD12NF06LT4

STD12NF06LT4,Is there a "G" marking on the right top corner of the part? How can we read the DC from label? Thank you.

RHFL7913A negative LDO regulator current limit adjustment

Hi,I have a problem of adjusting the RHFL7913A negative LDO regulator current limit to about 0.5A by a Rsh resistor. I tried with 12.4 kOhm but no current limitation is seen even at around 910 mA load. Anyone happen to know the correct resistance val...

mijuhi by Associate II
  • 2762 Views
  • 6 replies
  • 0 kudos

Resolved! FERD20H100S MTBF and FIT Reliability Metrics

Hello, I am trying to find reliability data (specifically MTBF and FIT) for the FERD20H100S. If anyone knows where to find it or could point me in the right direction I would be very grateful.Thank you,-M

TMil28 by Associate
  • 1160 Views
  • 1 replies
  • 0 kudos

STM32L0 boot sometimes fails on battery power - intermittent issue

I have an STM32L0 project that operates from a CR2032 coin cell battery. The board operates fine most of the time but there have been a few occassions where the power cuts out after a couple of hours or so and then the board will fail to boot up with...

J83 by Associate
  • 1611 Views
  • 0 replies
  • 0 kudos

STUSB1602 - Documentation request

Is there any documentation regarding the I2C registers of the STUSB1602 and the SPI interface?I cannot find information regarding the SPI interface anywhere, other then maybe reverse-engineering the driver.Is this available anywhere?

sgetaz by Associate
  • 1015 Views
  • 1 replies
  • 0 kudos

Resolved! I’m trying to identify an ST component.

I’m trying to find a replacement for this device from a light dimmer. I think it’s a triac, but the numbers on the front don’t match any search results, other than a similar request on this forum, so I’m hoping that someone can help!   

IMG_0134.jpeg
OrrinC by Associate
  • 3612 Views
  • 5 replies
  • 2 kudos

TRIACs for Home AC Switching using T2035T-8G

I have been using the "Triac, SCR and ACS Simulator" to simulate the activation of a 10 Amperes load with T2035T-8G (as I am having issues with this component) and I was wondering why it shows a Tj extremly high (388ºC) if this device could handle 20...

domoticsolution_0-1695686444448.png domoticsolution_1-1695686634832.png domoticsolution_2-1695686649760.png