cancel
Showing results for 
Search instead for 
Did you mean: 

SPSB081-Component Datasheet

SandeepPiduru
Associate

I am working on SPSB081 power management control IC. I need support in the following points:

1. which revision of data sheet to be followed, because there are some discrepancies in register set(addresses) of revision 2 datasheet.

2. for refreshing the watchdog, TRIG bit should be toggled every time within safe window(7.5 to 12 ms in configuration1, 37.5 to 60ms in configuration2), though i am toggling the TRIG bit of CR1 register for every 50ms, still the NRESET pin is toggling which means reset is happening. 

can some one help me in the above points???

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0