Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Looking for API access for the L99LDLH32

Hi, I am looking for a way to send messages to a L99LDLH32 board via another program. I found the STSW-EVLDLH32GEN, but this seems to allow only to manually set select messages. What I need is to be able to determine the values programmatically and w...

jluberb by Associate
  • 991 Views
  • 0 replies
  • 0 kudos

Resolved! L6470 Stepper Motor Driver Vreg No voltage

I have attached two images of the L6470 Motor diver, In the new design PCB the motor drivers are heating up and don't seem to respond to SPI commands. No voltage is present on the VREG pin. The sense resistors were added basically for measuring the w...

Label format

Hello, I have Part number STD10P6F6, I received these parts with a ST micro label on them. This label holds the trace code and at the bottom of the label it says LOT, Followed by a code. I assume that is the lot code for the parts, can you please cla...

EVLONE65W pd charger not work

hi sir ,we are working on EVLONE65W pd charger .we are facing issue in the circuit .output is not stable at secondary outside.can we know what we are doing wrong in the circuit ?

STPM066S OTP Programming Application Note / Example Code

Hello,I am trying to set up an STPM066S PMIC via OTP (One Time Programming), but without success so far.I am struggling a bit with the description in section 6.7 of the STPM066S data sheet (Rev. 2).a) Is a more detailed application note on OTP availa...

csuel by Associate
  • 1333 Views
  • 1 replies
  • 0 kudos

30W Flyback AC/DC Converter with PFC and isolated output

Hello,I have to design a power supply for our new product. I would like to implement this with a flyback converter. The biggest las on our board is the IMX.8, this changes its power profile depending on the requirements.Key points of my design:- 230V...

NWizz.1 by Associate
  • 1142 Views
  • 0 replies
  • 0 kudos

Resolved! I need a help to identify this part

Hello! I have two components (in SMB package probably). The markings are:1) ME G3 202 (no polarity stripe on package)2) EE G3 223 (with polarity stripe)Can you help me decipher what these elements may be and what may be the difference between ME and ...

ME G3 202.png EE 63 223.png
Proboszcz by Associate II
  • 2807 Views
  • 2 replies
  • 1 kudos

LD1086 DPAK pin configuration

Do we have a clear Pin Numbering configuration for this component as pin numbering which is 1,2,3 the datasheet did not clarify clearly.

Sakura_1-1697430392926.png
Sakura by Associate
  • 1263 Views
  • 1 replies
  • 0 kudos