User Activity

Hi Experts, I want to reset the ST32F303E-EVAL to default FW, where could I get the FW to download ?
Hi Expert, I wan to use STM32303E-EVAL + STEVAL-IPM15B 3Sh to run the motor profiler 5.4.8.But the error message is shown below.I connect the control board to PC via USB, the LD8 is red. The device manager of PC cannot see com port. I think the STM32...
Hi Experts, I wonder to know if this kit is suitable for me to develop with my motor. ​Below is my motor's spec.Pole : 8Rated Power : 10KWRated DC : 220VRated Current : 31.5ARPM 3000If yes, does this kit include sample code?