Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why my STGIPS10C60-H has no output voltage

When using the chip GIPS30C60-H, sometimes the three-phase bridge switching signal is given but there is no output, regardless of whether the SD/OD pin is set high or not. This chip is used in a motor controller with a 0-270V DC bus supply and input ...

CSLx30 by Associate
  • 1022 Views
  • 1 replies
  • 1 kudos

Resolved! LM317 丝印

能具体说明第二三行,代表的是什么呢? 

lm317.jpg
nygjp by Associate
  • 1092 Views
  • 1 replies
  • 1 kudos

VN7004SLH 4-layer board design example on datasheet

On p23 Fig 35 of https://www.st.com/resource/en/datasheet/vn7004slh.pdf, Are the big copper areas on the 4-layer PCB around the IC GND or VCC?  The figure seems to be GND, but how can GND help dissipate the heat from the ICs if the thermal vias are c...

jsmith by Associate II
  • 1597 Views
  • 2 replies
  • 0 kudos

LTSPICE model of STL210N4F7AG for Thermal modelling not working

Hello,I am trying to create the thermal model of Buck boost converter for my 20V application. I found STL210N4F7AG from ST with low Rds_on available on market. I dowloaded the spice model and created a symbol based out of V3lib file. I put it in my m...

DCDC_BuckBoost_using_STL210N4F7AG.png
Nagella by Associate
  • 1151 Views
  • 0 replies
  • 0 kudos

Output current limit for RHFL6000A

Hi All, In this LDO the output current limit can be set by a Rshort resistor from pin 8 to V_in.Is there any formula for the calculation of such a resistor? On the Figure 19 in the datasheet there is a plot showing Short-circuit current vs RSHORT for...

ozf by Associate
  • 865 Views
  • 1 replies
  • 0 kudos

power output is like AC in stpm34

I use stpm34. stpm34 reads voltage and current as rms. but stpm34 read active/reactive power like ac.I think stpm34 should read them like dc. is it right? I wanna dc value of active/reactive power.Could you help me? 

GyeongilKim_0-1701322676023.png

Resolved! STBC15 wiring of open drain output pins

Hello, I see there are two open drain output pins on the STBC15: CHGINOK and PG. If I don’t need to read the CHGINOK and PG status, can they either be left floating or connected to ground, without needing to add an external pullup? Please confirm if ...

EC.3 by Associate III
  • 1007 Views
  • 1 replies
  • 0 kudos

What is the difference between the LM211 and LM311

The datasheet says that LM211D/DT has a temperature of -40 °C, +105 °C and output to negative supply voltage 50VLM311D/DT has a temperature of -0 °C, +70 °C and output to negative supply voltage 40VIs there any differences in performance or electrica...

jgananam by Associate
  • 1237 Views
  • 1 replies
  • 0 kudos

Resolved! TCPP03-M20 using Mosfet driver outputs for logic control

Hello,I'm using TCPP03 for a DRP solution. For my design it would be good to use the Mosfet drivers for controlling a logic input for further power control instead of using Mosfets. Is it possible to use the gatedrivers with the SRC-pins connected to...

mikeho by Associate
  • 1447 Views
  • 1 replies
  • 1 kudos