cancel
Showing results for 
Search instead for 
Did you mean: 

TS33 datasheet mentions that it supports 1.8V fixed output voltage too, but cannot find relevant ordering code.

NPAL.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @NPAL.1​, to the community!

Unfortunately, the first overview page of the data sheet indicates voltages that are not currently supported. However, the information is relevant in the data sheet, section 7 (Ordering Information):

  • 1.25V
  • 2.048V
  • 2.5V
  • 3.0V
  • 3.3V

That means, 1.8V, 4.096V and 5V are not (yet) available.

And if you want to ask now when this will be the case - that is currently unpredictable.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.