cancel
Showing results for 
Search instead for 
Did you mean: 

SW4ST build of X-CUBE-SPN7 demo project

jgreg.blair9
Associate II
Posted on June 11, 2017 at 20:47

build using 

&sharpen.X-CUBE-SPN7.zip

 

Running an up-to-date Eclipse Ac6 session here is what happens when I try to build the &sharpX-CUBE-SPN7 demo application:

1.select  File menu item

2.   select Open Projects from File System

3.     select Import Projects from File System or Archive

4.      click 'Archive...'

5.        choose file 'en.X-CUBE-SPN7.zip' and click 'open'

6.          displays 'en.X-CUBE-SPN7.zip_expanded' + 4 Nucleo 030/103/302/401 projects click 'Finish'

An internal error occurred during:'C/C++ Indexer'

Details are:

  An internal error occurred during: 'C/C++ Indexer'.

  org.eclipse.cdt.internal.core.pdom.PDOMProxy cannot be

  cast to

  org.eclipse.cdt.internal.core.index.IWritableIndexFragment

7. click OK

8. Right click on 'STM32F302R8-Nucleo Configuration' in Project Explorer tab

9. select 'Build Project' from drop down list

An internal error occurred during:'C/C++ Indexer'

Details are:

  An internal error occurred during: 'C/C++ Indexer'.

  org.eclipse.cdt.internal.core.pdom.PDOMProxy cannot be

  cast to

  org.eclipse.cdt.internal.core.index.IWritableIndexFragment

- same error as before.  Click 'OK'

The Problems tab displays:

Description    Resource    Path    Location    Type

make: *** No rule to make target `C:/Users/giuseppe scuderi-sl/Desktop/MOTOR CONTROL/Peppe/trunk/Firmware/X-CUBE-SPN7-MC-6STEP/Middlewares/ST/UART_serial_com/Src/UART_UI.c', needed by `Middlewares/UART_serial_com/UART_UI.o'.  Stop.    STM32F401RE-Nucleo Configuration             C/C++ Problem

make: *** No rule to make target `C:/Users/giuseppe scuderi-sl/Desktop/MOTOR CONTROL/Peppe/trunk/Firmware/X-CUBE-SPN7-MC-6STEP/Projects/Multi/Examples/MotorControl/Src/main_F302.c', needed by `user/main_F302.o'.  Stop.    STM32F302R8-Nucleo             C/C++ Problem

Repeating steps 8 and 9 selecting 'STM32F401RE-Nucleo Configuration' produces identical results.

Analyzing the error message, the projects appear to have a hard path in the the project path

'C:/Users/giuseppe scuderi-sl/Desktop/MOTOR CONTROL/Peppe/trunk/Firmware/X-CUBE-SPN7-MC-6STEP/...'

I want to build the project.  First I need to load it into Eclipse. 

How do I load the en.X-CUBE-SPN7.zip demo project into SW4ST Eclipse so the file paths are properly updated?

Failing that, how can I manually update the file paths?

#sw4st #ihm07a1
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Limespace
Associate
Posted on June 12, 2017 at 09:32

I replaced 'C:/Users/giuseppe scuderi-sl/Desktop/MOTOR CONTROL/Peppe/trunk/Firmware/X-CUBE-SPN7-MC-6STEP/' by 'PARENT-6-PROJECT_LOC/' in the .project file before importing it into the Workbench. This way it uses relative paths.

Khouloud GARSI
ST Employee
Posted on June 20, 2017 at 17:09

Hi

Blair.Greg

‌,

Please use relative paths as mentioned by

limespace

.

The issue is already highlighted internally and will be corrected on the coming version of the package.

Sorry for any inconvenience this may have caused.

Khouloud.

Posted on June 21, 2017 at 04:38

Thanks for the tip on changing the project file to denote the file

locations. That suggestion worked. The 302R8 code compiles with the patch

to the project file applied.

However it is too big for a 302R8. The compiled code .bin file size is 78K.

The supplied .bin and .hex files supplied in folder

STM32CubeExpansion_SPN7_V1.0.0/Projects/Mulit/Examples/MotorControl/Binary/STM32F302R8-Nucleo

as the reference build sizes are 24 K for the .bin file and 67 K for the

.hex file.

I can program the F302R8 with the reference build 24K .bin file. I

cannot program the target with the 78K compiled .bin file.

Suggestions?

On Tue, Jun 20, 2017 at 11:10 AM, Khouloud G <st-microelectronics@jiveon.com

Posted on July 23, 2017 at 12:02

Hi

Have you found a solution for this problem?

jgreg.blair9
Associate II
Posted on September 28, 2017 at 02:25

The 1.1.0 release of SPN7 on the website resolves two issues:

1.  Importing the project sets up correct file paths so the project can be built.

2. SW4ST/Ac6 builds a F302R8 binary file that fits in the F302R8 memory.  ST-Link can now program the F302R8.

The default 6-step BLDC project now spins the IMH001 motor.

>The default 6-step BLDC project now spins the IMH001 motor.

I am having a different experience. The example code and binary both give me a stuttering, sputtering, non-spinning motor.

 Never mind, jumper error on my part.