STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Command “ alsamixer�? doesn't work in SDK "en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15"

root@stm32mp1:~# uname -a Linux stm32mp1 5.15.24 #1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 armv7l armv7l armv7l GNU/Linux root@stm32mp1:~# pacmd list-sinks-inputs No PulseAudio daemon running, or not running as session daemon. root@stm32mp1:~# alsa...

mteaching by Associate III
  • 4388 Views
  • 2 replies
  • 0 kudos

How to Start Usb2 from u-boot?

hi, i'm stuck starting usbh_hs2 from u-booti can already start usbh_hs1 at boot, in order to load kernel and fs from an usb mass storage. i wish to do the same with usb_hs2, is that possible? is one configuration from DTS or from U-boot source code? ...

MBell.5 by Associate III
  • 2536 Views
  • 3 replies
  • 1 kudos

Using HAL_RTC in TouchGFX

Hello All,forgive me if this as an obvious mistake but I'm completely new to TouchGFX. I'm using STM32 MPU, with Cube, FreeRTOS and TouchGFXI have created a page in TouchGFX using the digital clock object, I have created a TickEvent to update the clo...

DPyke.1 by Associate
  • 1998 Views
  • 1 replies
  • 0 kudos

Resolved! multiple definition of `SysTick_Handler'

Hello,I created a new project in STM32CubeIDE for my STM32MP157A by using STM32CubeMX. In it I enabled UART and FreeRTOS on CMSIS-RTOSv2 and that's all. I use the auto generated code.Then I wanted to use TraceAlyzer on top of FreeRTOS however, upon i...

Fnx_QT by Associate III
  • 8541 Views
  • 6 replies
  • 0 kudos

GCNano GPU stack

I'm testing the Developer Package for STM32MP157c-dk2 demo board. Starter Pack is installed. When I compile the kernel as described in the Dev. Package's "README_HOW_TO.txt" file and update the kernel, The "Cube" example ceases running. It only says...

Ronte.1 by Associate III
  • 5069 Views
  • 6 replies
  • 0 kudos