User Activity

Hello,my system is based on an STM32MP151x, running embedded Linux (Buildroot generated + all the ST patches, v5.3.56). I am suing an SPI connection to an external hardware but so far, i am not able to set the SPI clock to 20MHz and higher.Looking at...
I am using an STM32MP151 in linux (5.4.56) and therefore using the DTS to setup some GPIOs i need.I have difficulties setting up PUSH_PULL | PULL_UP configuration in the DTS for my GPIO, while, after linux has booted, using devmem i am successfull in...
Hello, my EVB is based on STM32MP151A SoC. The situation we are facing is that sometimes, the FSBL gets stuck and we would like to recover from it. i.e. reflash some Known Good FSBL.   As the FSBL in that situation is kinda functional, the device wil...
I apologize in advance as the question is really a basic and obvious one ... My custom board is using an STM32MP151 SoC.Is it possible to re-write programmed OTP bits (namely, OTP Word 3 for boot modes).My feeling is that, this is not possible (One T...