STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX breaks TF-A

When building a custom machine for the STM32MP153AAC (using yocto), the device tree generated by CubeMX for the TF-A creates the following output:NOTICE: CPU: STM32MP153AAB Rev.B NOTICE: Model: STMicroelectronics custom STM32CubeMX board INFO: R...

Yocto building , tf-a & u-boot

Hi STµ Teams!Another questions!I'd like to have some precisions about yocto building :I 'm able to build st-image-core, SDK1.2.--Does the u-boot (and tfa) is built each time (ie: fetching sources, applying patch, compiling) when I'm bitbaking or does...

Eldam by Senior
  • 1721 Views
  • 1 replies
  • 0 kudos

Resolved! st-image_core & M4 copro

Hi ST Teams,I'm building successfuly an image "st-image-core", for stm32mp1 machine.I'm able to add python package and remove some package too.But unfortunately, My team who works on M4 copro can't connect anymore on it.If i made a sd card with start...

Eldam by Senior
  • 1717 Views
  • 2 replies
  • 0 kudos

Resolved! Openstlinux and STM32CubeProgrammer

Hi, I try upload Openstlinux-5.4-dunfell-mp1-20-06-24 in a stm32mp157c-ev1(Nand).I used STM32_Programmer_CLI version 2.3.0 and I get the next error:------------------------STM32_Programmer_CLI ---------------------------------reconnecting the device ...

AVazquez by Associate III
  • 2946 Views
  • 4 replies
  • 0 kudos

u-boot and kernel dependency

Hi All.I am currently using STM32MP15-Ecosystem-v1.2.0. for DK2. At the moment I don't plan to completely upgrade to v2.0.0 but I would like to test the new kernel version (5.4.31). I have compiled the new kernel version and a new device tree but onc...

AVazquez by Associate III
  • 3502 Views
  • 5 replies
  • 0 kudos