2020-09-25 8:54 AM
When building a custom machine for the STM32MP153AAC (using yocto), the device tree generated by CubeMX for the TF-A creates the following output:
NOTICE: CPU: STM32MP153AAB Rev.B
NOTICE: Model: STMicroelectronics custom STM32CubeMX board
INFO: Reset reason (0x14):
INFO: Pad Reset from NRST
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.2-r1.0(release):devtool-patched-dirty
NOTICE: BL2: Built : 13:15:56, Sep 25 2020
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x10000000 (256 MB)
INFO: BL2 runs SP_MIN setup
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffed000
INFO: Image id=4 loaded: 0x2ffed000 - 0x2ffff000
INFO: BL2: Loading image id 5
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 0
INFO: address 0x2ffe5928
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 0
INFO: address 0x2ffe5928
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: Start Download partition 0 to address 0xc0000000 length 0
INFO: USB : DFU : end of download partition : 0
INFO: Loading image id=5 at address 0xc0100000
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 3
INFO: address 0x2ffe5928
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: receive request 6
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 3
INFO: address 0x2ffe5928
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: usb_partition_size: partition size : 0xce9cf
INFO: Start Download partition 3 to address 0xc0100000 length 846287
INFO: USB : DFU : end of download partition : 3
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 0
INFO: address 0xffffffff
INFO: Send detach request
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: Receive Detach
INFO: Image id=5 loaded: 0xc0100000 - 0xc01ce9cf
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffed000
INFO: SPSR = 0x1d3This is as far as it gets. The CPU appears to hang here.
After an extremely tiring and timely process of diffing/binary searching the TF-A device tree with one that works, I have found that adding the following to the generated TF-A device tree fixes the issue:
/* USER CODE BEGIN addons */
&cpu0 {
cpu-supply = <&v1v2_vdd_core>;
};
&cpu1 {
cpu-supply = <&v1v2_vdd_core>;
};
/* USER CODE END addons */Where v1v2_vdd_core is a node in the pmic section:
pmic: stpmic@33 {
compatible = "st,stpmic1";
/* (stuff) */
regulators {
v1v2_vdd_core: buck1 {
regulator-name = "v1v2_vdd_core";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-initial-mode = <0>;
regulator-over-current-protection;
lp-stop {
regulator-on-in-suspend;
regulator-suspend-microvolt = <1200000>;
};
standby-ddr-sr {
regulator-off-in-suspend;
};
standby-ddr-off {
regulator-off-in-suspend;
};
};
/* (more stuff) */
};
};I don't understand why this fixes it, nor do I understand why it hangs in the first place.
If you need more information I'd be happy to supply it.
2020-09-28 1:33 AM
Hi @AMurr.2282 ,
You may know that for "sample" project as you ( STM32MP153AAC ) STM32CubeMX generate only "partial" Device Tree.
You need to fill all USER SECTION in order to get a complete and bootable Device Tree.
To help you we provide this wiki page :
https://wiki.st.com/stm32mpu/wiki/How_to_create_your_board_device_tree
+ you can use complete dts generated in case of project for DK2 or EV1 board in order to help how to fill USER SECTION
Hope it help
Olivier