Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L9369's problem shooting

Hello. I'm using L9369 IC and have a problem.   Stage A is not working.   i made control code for Stage A,B. (they are very similar)   i used below two command for H-brdige operation.   but. current was not flow.   here is phenomenon. 1.Low side GL1,...

0693W00000aIBOdQAO.png 0693W00000aIBS6QAO.png 0693W00000aIBSVQA4.png
ldong.1 by Associate III
  • 2391 Views
  • 3 replies
  • 1 kudos

Poor PF at light loads

We are designing PFC converter using L6562A controller for 340Vac-440Vac to 665Vdc with 250W as output power.We are facing problems of very low Power factor at lighter loads.What might be the possible reasons for this and how can we tackel this? Rega...

dvramgir by Associate
  • 866 Views
  • 1 replies
  • 0 kudos

Resolved! About the TS33 series

I don't know the internal structure of the TS3330AMR IC.Is there a functional block diagram of the IC's internal structure?

Ikegawa by Associate
  • 736 Views
  • 1 replies
  • 0 kudos

Resolved! STUSB4710A output not stable

I developed a multi-port charger with multiple STUSB4710A and companion ST1S14PHR with the recommended bill of materials. The evaluation kit worked fine however my board does not work consistently. I read back the status register and detecting underv...

l7987l Arcing across soft start pin

Hi,L7987L IC is used for generating -15V from 24V supply. it was working OK up to 12V, upon further increasing Supply Voltage we found arc at the soft start pin.

Dina by Associate
  • 704 Views
  • 1 replies
  • 1 kudos

[L9369] when to set RST function enable on EN_EL pin (#47)

EN_EL pin (#47) is originally EN function and to set it as RST function, need to set D[4] of reg8Ah. My question: When to set D[4] to 1 to enable RST function?  should it do after setting watchdog ? Thanks!    RST Remapping on EN_EL the function of I...

haihun by Associate II
  • 830 Views
  • 1 replies
  • 0 kudos

L6599 Protection

 Hi.I am using the L6599AD without PFC.Previously, the DIS pin was connected to the DELAY pin and used as a SHUTDOWN.However, the frequent peak current caused SHUTDOWN.So I connected the DIS pin to GROUND and made it work in HICCUP MODE.However, the ...

JK5 by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos