User Activity

Hey,so I was trying to use the VND7020AJ as a driver to loads,and wanted to power the load to 7.2V while powering the high side driver with 12V.Im using a stm32f103rb,and using an outpin pin timer to control the pulse width to the input pin on the dr...
Hey I was I wondering if it was possible to use the x-nucleo-ihm08m1 on an 144 board.I only have 144 pin boards but couldnt find my board on MC Workbench.I also tried the motor pilot software and it said to configure the board.I suppose I can use it ...
Hey, probably a dumb question, but I couldn’t find it in the datasheet. Can each pin of the VNQ9025AJ handle 30A, or is that the rating for the smart switch as a whole with a limit on each pin? Honestly, I’m hesitant to believe a single pin can handl...
Hey,I'm planning to use this high-side driver in a project distribution module, but I'm having trouble fully understanding how the current sensing works.I've looked at the schematic, and I see a combination of two resistors, Rprot and Rsense. Is this...
 Hey,I'm planning on building an ETC to control a throttle valve using the L9960 H-bridge. I'm currently in the process of designing a PCB for it. The driver is supposed to have 12V as VsV_sVs​ and handle up to 10A max as output load. The PCB I'm des...