Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6207 - Cboost connetion

Posted on August 27, 2013 at 02:52 According to the datasheet, Cboost(220nF/100V) is connected between VBOOST pin and VS pin. But according to the EVKIT schematic, Cboost is connected between VBOOST pin and GND. Which connection is more recommended...

k-takagi by Associate
  • 692 Views
  • 1 replies
  • 0 kudos

PMSM FW v3.2 with tacho output

Posted on August 22, 2013 at 11:10Hi I am a PMSM FOC v3.2 user. How can i output tacho pulse which its frequency is propotional with rotor speed. MCU is STM32F103CB in senserless Cordic.  Thanks in advance.  

supakit by Associate II
  • 1014 Views
  • 2 replies
  • 0 kudos

STEVAL-IFN003V1

Posted on August 24, 2013 at 20:33Hi,I am trying to get sensorless FOC working on a 14 pole surface mounted outrunner motor. It has a Rs of 0.35 Ohm and Ls of 1.0 mH.I installed Motor Library v3.0 and applied the IFN003V1 patch. I set all of the boa...

joe2 by Associate II
  • 1295 Views
  • 3 replies
  • 0 kudos

Pspice models of ST MOSFETs

Posted on August 28, 2013 at 15:12The models are available on ST website but there is no documentation as to understand the model or use it. The thermal + electrical model has case and junction temperature, but do not know how to use these terminals...

praveen by Associate
  • 975 Views
  • 0 replies
  • 0 kudos

FOC + PFC

Posted on June 11, 2013 at 10:50For a motor control project I must use active power-factor-correction (PFC). Is there any sample code / sample project how to do that with STM32? Any suggestions what development kit to use? There is the STEVAL-IHM034...

STM32F40G-Eval

Posted on April 15, 2013 at 17:30Hi, Am having this error, #error ''Please select first the Evaluation board used in your application (in Project Options)''    i commented   /* #define STM32F427X */ in STM32F44XX.h but i still have this error , how...

STM8S BLDC Speed Closed Loop runaway issue

Posted on August 19, 2013 at 05:13Hi, I am using STM8S three-phase BLDC motor control software library V1.0 to drive BLDC. Everything works great except PI regulator for speed closed loop runways after speed 13000rpm. My settings are: &sharpdefine...