cancel
Showing results for 
Search instead for 
Did you mean: 

PMSM FW v3.2 with tacho output

supakit
Associate II
Posted on August 22, 2013 at 11:10

Hi

I am a PMSM FOC v3.2 user.

How can i output tacho pulse which its frequency is propotional with rotor speed.

MCU is STM32F103CB in senserless Cordic. 

Thanks in advance.

 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Gigi
ST Employee
Posted on August 26, 2013 at 14:33

Ciao,

can you explain better your request?

What do you mean with the following question?

 

How can I output tacho pulse which its frequency is propotional with rotor speed.

 

Ciao

Gigi

supakit
Associate II
Posted on August 30, 2013 at 16:04

Hi Gigi

it mean STM32 generates the pulse train which its frequency is propotional with rotor speed.

for example;

current rotor speed is 1,500RPM.

And STM32 will generate pulse train which its frequency is 100Hz. (4 pole pairs)

also 110Hz at 1,650RPM

This is a feature of Tacho Gen.

Thanks