error while using powerSTEP01,
Posted on March 14, 2017 at 17:05 when the stepper motor got horizontal forces the powerstep01shutdown and all the status register bits turns to zeros.We work in current mode, the thresholds levels adjusted to maximum.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Posted on March 14, 2017 at 17:05 when the stepper motor got horizontal forces the powerstep01shutdown and all the status register bits turns to zeros.We work in current mode, the thresholds levels adjusted to maximum.
Posted on March 15, 2017 at 08:171�what is Vsense_nom ? How level? I find nothing in datasheet.
Posted on March 09, 2017 at 15:28Hi, i designed transformerless capacitive power supply for compact home automation project. Initially its used for only controlling load so it worked good at 4.8Vdc. Later i added seven segment display and tactile sw...
Posted on February 17, 2017 at 06:01In the document EVLCMB1-90WADP, is L2 a simple inductor or a transformer? If it is a transformer, then what is the turns ratio?
Posted on February 21, 2017 at 07:11Hello,I am looking at using the L6480 in the externally supplied modes, where my system will be supplying: VS = +24V DCVSREG/VCC = +12VVCCREG/VREG = +3.3VThe +24V supplied to VS by the system is removed (floating)...
Posted on February 28, 2017 at 15:54i am looking at using the L6668 as a multy output flyback, i need it to have a high voltage start up (which this IC does have, that is good), but i also need it to synchronise it to about 100KHz from a micro.my qu...
Posted on February 18, 2017 at 17:51I am using the L6615 in a 50V bus current sharing application and I have the required voltage divider from each side of the high side current sense resistor to ground but I am unsure if another series resistor nee...
Posted on February 13, 2017 at 20:46I want to use the STM6600 controller to manage the power ON/OFF of my microcontroller system. In the specific I want:- Turn ON the system simply pushing a button.- Turn OFF the system simply pushing the same butto...
Posted on February 10, 2017 at 15:10HiI'm using the L6472 Eval board, revision 1.1.We got two L6472 Eval board connected to our main stm32f2 board. Both drivers are running smoothly and everything is working, but reading the absolute position regist...
Posted on February 08, 2017 at 15:03Hello,i our Motor Control Board with FOC i have very high losses in the Driver IC L6230Q in the VFQFPN package.In the On-Time of the High side i have a differenz of 2.6V between the Operatine Voltage (21V) and the...