Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power MOSFET Simulation Model

Posted on July 29, 2017 at 04:07Hello,I'm trying to simulate STP55NF06. You can download its model here: /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fpower-transistors%2Fstp55nf06.html.The pin 1,2, and 3 should be gate, drain, and source r...

0690X00000607gsQAA.png

Recommended pad layout for POWERSO36 package

Posted on July 28, 2017 at 19:23Is there a recommended pad layout for the POWERSO36 package? Ap note AN668 regarding this package has a detailed layout for the POWERSO20 package with measurement data, but not the POWERSO36.

Microstepping with L6208

Posted on July 24, 2017 at 09:41Hello,I am trying to implement microstepping on a X-NUCLEO-IHM05A1, which i am using with an Arduino uno. I have followed the microstepping application note, and i obtained the right waveforms at l6208 references' inp...

0690X00000603xtQAA.jpg 0690X00000603vFQAQ.jpg

smps parallel connection

Posted on July 19, 2017 at 12:15Hello. i design L6566BH on design süite. But i see that max power out is 350w. if i do same smps 3 pieces and i want to get 1050w can i connect their outputs in parallel connection? because i see that it is not basic...

powerstep01 with high voltage design

Posted on July 17, 2017 at 11:41I'm using http://www.st.com/content/st_com/en/products/ecosystems/stm32-open-development-environment/stm32-nucleo-expansion-boards/stm32-ode-move-actuate-hw/x-nucleo-ihm03a1.html to evaluate the powerstep01 chip, and ...

Resolved! L6480 Abnormal over current detection behaviour

Posted on April 10, 2017 at 09:44HiAbnormal over current detection behaviour on stepper motor controller L6480. After initialization a hard stop command is given to hold the stepper motor, which seems to work just fine, all the expected waveforms ap...

Surge Test Failure

Posted on July 13, 2017 at 06:50Dear Team,Please find the attached design. ehg7520_cpu_ board.pdf In my product design i have used TVS diodes and ORing diodes from ST Micro electronics. My product has to under go the following test. TEST_Cases.xls ....

STM32 PMSM FOC Software MC library:What is the impact of calling TSK_SafetyTask() at 1ms interval, instead of 0.5ms as recommended in User Manual?

Posted on July 12, 2017 at 12:23I'm using STM32 PMSM FOC Software MC library to run my motor. I use the MC API to interact with my own code and it seems to work fine - motor can run.However, mentioned in the User Manual (UM1052, section 10.3, Table ...

Boost LED Driver

Posted on July 03, 2017 at 12:13We are using LED6001 LED Driver in a Flasher.The problem is when the input is less than 10.5V it works O.K but when the input is more than 10.5V the LED current reduces to almost 10mA or shuts down. The Problem is sam...

ammar by Associate
  • 1262 Views
  • 1 replies
  • 0 kudos