Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST1S14 Vout=22v issue at Vin close to Dutycycle max

Posted on February 16, 2018 at 16:50Hello!I am facing a problem with ST1S14. Conditions: - if Vin is 24.5V or less and load current less 30mA, output voltage drops to about 15V. (Problem)- If Vin becomes about 16V and less and load current still les...

0690X00000609hwQAA.png

MOSFET and Ioslation transformer for UC3842B

Posted on March 08, 2018 at 14:09Anyone could comment on why for UC3842B design, the MOSFET and Isolation transformer gets hot . We have done all calculation as per the design theory calculations. Thanks!

EHD by Associate II
  • 661 Views
  • 0 replies
  • 0 kudos

STC3115 Not showing correct SoC after charging

Posted on September 12, 2017 at 12:02 Hello everyone, We are having an issue with STC3115 (fuel gauge) where we are charging our device while it is powered off. After powering on the device, SoC received from STC3115 driver to application shows t...

[ATT]11395

Posted on February 27, 2018 at 14:19Start-up failure FOC SDK Hello!I used STM32F103C8 + STEVAL-IP05F and I was able to run successfully.Now, I developed my PCB, in which I took STM32F072C8 and STGIPQ3H60T-HZ.  I used FOC4.3.When I try to start, aft...

H bridge VNH7100BAS monitoring

Posted on February 15, 2018 at 09:13Hello,I am trying to monitor the h bridge VNH7100BAS. I want to open HSA and LSB during a certain time then open LSA and LSB. But I do not succeed to do it. I use the tab 'Input A,B' and try to control the H-Bridg...

L6470 Cracked

Posted on February 26, 2018 at 15:16L6472 stepper driver.hello, we are using 4x L6472 driver chip on a single board for some time now. We used the internal 16MHz clock, but it appeared that the clock frequencies differ a lot from each other. Accordi...

Development Board for HFI

Posted on July 01, 2015 at 17:24Hello, I was at Embedded world Germany and an Italian ST representative showed me encoderless motor control which even worked well with zero speed (using High Frequency Injection). I want to test if this works in my c...

dwisse by Associate
  • 2399 Views
  • 5 replies
  • 0 kudos

What Gate Driver is built in the STSPIN32F0 ?

Posted on February 23, 2018 at 18:44Hi there,I would like to create a custom PCB build around the STSPIN32F0 MCU which integrates a gate driver and some other fancy features.Now I need to know some specs of that driver but they're not listed in the ...

Mad Max by Associate
  • 832 Views
  • 0 replies
  • 0 kudos

TDA7850EP - what is that?

Posted on February 01, 2018 at 14:15Hello!Our company recieved from the official dealer in our country the TDA7850EP chip. The seller claims that this is an improved version of the TDA7850, but we never heard about. Is it so?I did not find informati...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.