Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Motor Driver IC

Posted on March 23, 2018 at 08:13Hi Community,We have planned to use L298P motor driver IC in one of the project.Can his part support for medical applications ???Please suggest the part, with similar specifications and applicable for Medical applica...

Motor Control Library maximum modulation index

Posted on March 21, 2018 at 10:37Hi,I have question about maximum modulation index in motor control library. When it is 100% is there any danger at very low RPM high side driver's bootstrap capacitors to be completely discharged? Is there any mechan...

mosfet stp5nk50z

Posted on March 13, 2018 at 18:21HelloI am looking for an equivalent of the mosfet stp5nk50z to 220  for a Rolling shutter, thank you

SM30T21AY: MTBF Report / FIT

Posted on March 14, 2018 at 16:29Hello,I am looking for the MTBF Report of FIT value for the following part: SM30T21AYThank you for your help!

X-Cube-SPN8: CubeMX .ioc file available?

Posted on March 14, 2018 at 23:20Hi,I want to build my own application based on the X-Cube-SPN8 BLDC motor control expansion package.I can't find the CubeMX .ioc files in this package. However this would be very helpful as a starting point.I also ch...

Qi Receiver-Induction Coil Design

Posted on March 13, 2018 at 11:46I want to design Qi wireless receiver with 7.5W output capacity. I will use device STWLC03JR.Can anyone suggest me compact designing criteria or specification for Induction coil.I have seen they are readily available...

K_P_D by Associate II
  • 783 Views
  • 0 replies
  • 0 kudos

powerstep01 spi baudrate setting problem

Posted on March 09, 2018 at 14:05Hello,we tried to communicate to the powerstep01 trough spi and with a baudrate of 500kHz everythink works fine.The problem occur if we set the baudrate above 500kHz. Then we lose the first bit of each byte.For examp...