Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IHM02A1 L6470 muliple Boards

Posted on December 01, 2017 at 17:25Hello,I currently try to use more than one Stepper Motor Controller Board (3 to be precise) stacked. Every single one is working perfect with individual CS jumpers set by using the standard library from st - using...

0690X000006096RQAQ.png 0690X00000608xlQAA.png

RHFL7913 negative Regulator, Current programming

Hello ST,In the process of testing the RHFL7913 device, I would like to program the current limit for the device. Though datasheet says device is internally programmed to 4A. I would to reduce the current capability to 2A by placing the resistor ( i...

SM.11 by Associate
  • 782 Views
  • 0 replies
  • 0 kudos

Partial charge with STBC15 ?

I can not do the partial charge with STBC15. For example, when the battery is in the BSP state (system is powered by the battery) and the Vbat is 3.8V, if I plug the charger then unplug the charger after some seconds, the Vout is off (0V) ! This is ...

ENGUY by Associate
  • 579 Views
  • 0 replies
  • 0 kudos