Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Internal comparator OCP circuit

Hi, may I ask can move the internal comparator OCP circuit which is placed in low side MOSFET driving stage to between high side and low side MOSFET with maintain the current same firmware setting which is in ESC001V1 reference design​

Current control for L6482H at low speeds

Hello,I am developing a motor driver solution for a medical device. L648x seems to be a good option considering the current control for gate driver (which in my case will help reducing EM emissions). I already tried L6480 but I was experiencing a lot...

0690X000006DgaGQAS.bmp 0690X000006DgaBQAS.bmp
FOliv.15 by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

Working with the PowerStep01 and have run into a question regarding the minimum tick clock speed input. The documentation seems to indicate 4MHz but I can not find a min value.

The purpose of this is to determine if I can run the motor slower than approx. 15 steps/s which is the slowest possible with a 4 MHz tick. This is at the maximum microstep of 128. Considering a change to STSPIN220, lower current and voltage spec but ...

JOrre by Associate
  • 786 Views
  • 0 replies
  • 0 kudos

Monitoring ISB039V1.

Hi,We are researchers trying to use the ISB039V1T for an inductive charging application. In the past, we have worked with ISB045V1T and used the STWBC GUI with the STEVAL_WBCDNGV1 to flash firmware updates and monitor the board's charging status. How...

YDesh by Associate
  • 561 Views
  • 0 replies
  • 0 kudos

No Output from EVALPWD13F60 board

We applied VCC1 & VCC2 @12V , VS = 110V, HIN1=3.3V, LIN2=3.3V (HIN2=GND & LIN1=GND) Measured output voltage across OUT1 & OUT2. However, no output voltage is observed. And also tried HIN2=3.3V, LIN1=3.3V (HIN1=GND & LIN2=GND). Here also same no outpu...

rmshub by Associate II
  • 962 Views
  • 1 replies
  • 0 kudos

We are using EVALPWD13F60. We are unable to make motor turn on.

We are using EVALPWD13F60. We are unable to make motor turn on. While we give pwm(10KHz) to HIN1 and LIN2 with different duty cycles by putting LIN1 and HIN2 as low , we getting 6 V as output. When we give HIN1 and LIN2 full time high voltage is drop...

APadm by Associate
  • 958 Views
  • 1 replies
  • 0 kudos