2018-05-17 6:24 AM
I would need advice on how to make a stepper motor drive with a supply voltage of 120Vdc and a current of 6 nominal Amps.
It seems to me there are only 2 ways, even if I do not know if they are feasible, they are:
1)
Use 2 PWD13F60 (2 H-bridges) to control the 2 windings of the stepper for the power part;
and use an STM32 microcontroller for the control part.
Sore point of this solution, I have not found any application notes that describe how to use the devices of the STM32 to directly control a stepper.
2)
Use 2 PWD13F60 (2 H-bridges) to control the 2 windings of the stepper for the power part;
and use an L6480 or L6482 controller for control.
Sore point of this solution, I do not know if the controllers that serve to directly drive the mosfet can be used only as 'digital' signals to drive the 2 H-bridges (which have already integrated the drivers).
Can someone help me on both questions or seal something else?
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.