Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help to identify PS

Hi all,Is anybody known something about this power supply? What I know is:There is an ST logo on the board.Input: ~240VACOutput: 12VDCusing 1NK60Z and TL431 in TO92 packageThere are four component blown out. One of the blown out 3 pin component marki...

0690X000008j49cQAA.jpg 0690X000008j49XQAQ.jpg 0690X000008j49hQAA.jpg
anagy9 by Associate II
  • 1073 Views
  • 1 replies
  • 0 kudos

L6227Q_VREF and OCD implement

I have PWM to control motor at each channel. One is limited by 0.3A and the other one is limited by 0.1A by voltage divider reference to 5V. By using this approach, as my understand I can not reach to OCD feature because the current can not reach to...

NHuy.12 by Associate
  • 703 Views
  • 0 replies
  • 0 kudos

STIB1060DM2T-L Does the IC have isolation for the microcontroller signals or should we add external optocouplers to protect it.

I am currently planning on build a low voltage 3 phase AC power supply for powering my DIY axial motor. I am scared if I input high voltage say 60V, it may have a chance of leak of current going to the micro-controller. I cant find any protection men...

SLi.1 by Associate
  • 839 Views
  • 0 replies
  • 0 kudos

Phase current control for L6470h

Hi dear,I designed a step motor driver board with L6470h and tested it. There are some problems with the board.I set the run current, hold current, ACC, ACC current, DEC, DEC current at the fixed value, and then changed the MAX speed, then the actual...

KFan by Associate
  • 689 Views
  • 1 replies
  • 0 kudos

I want to know how much time delay there will be between the comparative output matching and the pin output. Is the delay fixed?

Using STM32F407 comparative output function, we generate 57600Hz square wave. I find that there are some fluctuations in square wave. Observed by oscilloscope, the rising and falling edges of square wave have several ns fluctuations. So I want to kno...

sliu.0 by Associate
  • 590 Views
  • 0 replies
  • 0 kudos

L6470PD - Isolate Power Line

I am designing stepper driever using L6470PD.Is it possible to isolate system power and motor driver power?I wonder L6470PD internal connection. Is there related document?I want to design power line like the picture below

0690X000008iuK6QAI.png
yjong by Associate
  • 709 Views
  • 0 replies
  • 0 kudos

How to calculate the right Capacitor for Qi charging coil?

Dear Forum,currently I'm implementing a design with the STWLC33 and in the datasheet is a reference design for a coil with L = 8 uH and a C = 3.9 nF. I calculated the resulting resonance frequency and got about f = 90 kHz (with Cser and Cpar). Shoul...

EZueh by Associate
  • 772 Views
  • 0 replies
  • 0 kudos