Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Regarding STEVAL-SPIN3204

Purchased two (2) such boards (STEVAL-SPIN3204) from Digikey North America to evaluate the suitability of the SPIN32F0 for my automotive application.When attempting to download the eval software, I am trapped in an endless loop of "Error 403". In o...

JSang.13 by Associate
  • 644 Views
  • 0 replies
  • 0 kudos

Fill area for PM8803

I am planning to replace a faulty PM8803 POE SMD. I have never dealt with pads and fill areas before, so apologies for what is probably an incredibly basic question.The layout guidelines say:"The exposed pad of the PM8803 must be connected to VSS: de...

GOddy by Associate
  • 3837 Views
  • 0 replies
  • 0 kudos

What exactly is V_drop in the STP16DPPS05 datasheet?

I'm evaluating the use of STP16DPPS05 in my LED driving application.I'd like to drive two LEDs (wired in series) per channel at 5mA. The LEDs have a worst case forward voltage drop of 1.6V each. I intend to power the LEDs and the STP16DPPS05 with a 3...

0690X00000A9k2kQAB.png
greyltc by Associate
  • 3304 Views
  • 0 replies
  • 0 kudos

Resolved! STP08DP05 resistor R-EXT current

Background:In our application STP08DP05XTTR is supposed to drive six LEDs with 20mA constant current each using an external, 1 k-Ohm output current programming resistor connected to the R-EXT pin (pin 15). The LED supply voltage is 5Vdc.Question: Doe...

sinusoidal PWM control for PMSM motor

Hi friends,   I am working in electric vechicle controller segment. Already, I have done my bldc controller using six step ( trapezoidal ) control method. I was completed my project using STM32f103c8t6 controller.  I need to control the PMSM motor us...

Is the stps5l60sfy footprint PSMC (TO-277A) too big?

We got this picture from our PCB manufacture. They claim there is "too much footprint" for this component and it causes sliding of the part. The footprint is made with reference to page 6 of this document. https://www.st.com/resource/en/datasheet/stp...

0690X00000A9e6WQAR.png
DJC by Senior
  • 698 Views
  • 0 replies
  • 0 kudos

Signal sniffer

Hi everyone.I have a position encoder connected to a motor drive. The encoder transmit every 0.1ms a 73-bit data package using a protocol called EnDat 2.2 to the drive. The clock frequency is set to 5MHz, meaning one bit is 0.2 microsecond. Now I wan...

0690X00000A9ZljQAF.png
huy.pham by Associate
  • 2521 Views
  • 2 replies
  • 0 kudos