Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LDL1117S33R SCHEMATICS

Hello,I am using LDL1117S33R for one of my project. I want to convert 5 volt into 3.3V.Please find the attached schematics.Could you please verify the same ASAP?

0690X00000AqPFAQA3.jpg
AThom.17 by Associate II
  • 1212 Views
  • 2 replies
  • 0 kudos

ESC based on STEVAL-SPIN3201 and STSPIN32F0

Hello,I`m currently thinking of creating stripped down version of STEVAL-SPIN3201. I have a few questions before I can start with this project:Why is there STM32F103CBT6 MCU on the STEVAL-SPIN3201 evaluation board? I can`really see much purpose for t...

Margus by Associate
  • 1325 Views
  • 1 replies
  • 0 kudos

Hi all, We are using fuel guage IC: STC3117IJT . when powerdown mode is activated It consumes around 2mA, but it should be 1 uA. What can we do to minimize the shut down current in STC3117IJT? Regards, Nirav K.

While we have set the register REG_MODE to 0x0B as well as 0x01 to minimize the powerdown current but no luck.As shown in attached picture we have observed below scenario.1) the pulse of 50msec to 440uA by every 11sec  2) pulse of 240msec to 210uA by...

0690X00000ApTbDQAV.png 0690X00000ApTbIQAV.png
NKate by Associate
  • 601 Views
  • 0 replies
  • 0 kudos

Problems with changing the torque regulation torque

Hello,We have a problem with the controller wehn changing the torque regulation torque. This problem happens randomly but very frequent. When the motor stops we change the current regulation torque from 1300 mA to 250 mA. And some times we can see so...

YLoui by Associate
  • 644 Views
  • 0 replies
  • 0 kudos