2019-03-22 1:23 AM
Hi All;
I would like to calculate CT. I have formula below.
I factor = VREF / (AI * CALIB_I * DPOW * KSI * KINT )
VREF = 1.18 from datasheet
AI = 16 from datasheet
CALIB_i = 0.875 from datasheet
DPOW = removed
KSI = Rshut = 0.05 ohm when I calcurate from voltage Input vary 0.3V to -0.3V.
I adject 0.3V/5A = 0.06 ohm
KINT = 1 from datasheet
my I factor = 1.18 / ( 16 * 0.875 * 0.05 * 1 ) = 1,6857
nvmLeg_t metroDefault = {
{ // config
0x00000068
},
{ // data1[19] STPM (Config for CT)
0x040000a0,
0x240000a0,
0x000004e0,
0x00000000,
0x003ff800,
0x003ff800,
0x003ff800,
0x003ff800,
0x00000fff,
0x00000fff,
0x00000fff,
0x00000fff,
0x03270327,
0x03270327,
0x00000000,
0x00000000,
0x00000000,
0x00000000,
0x00004007,
},
{ // powerFact[2]
30154605,// , // ch 1 112,0028
19600493 // ch 2 //(1,18 *1,18 * (1+ (810000/470)) / (2 * 16 * 0.05 * 0,875 * 0,875) = 1960,04937
},
{ // voltageFact[2]
116274, // ch 1
116274 // ch 2
},
{ // currentFact[2]
//25934, // ch 1
25934,//,
16857 // ch 2 //1.18 / (16 * 0,875 * 0.05 * 1) = 1,6857
}
};When I use to CT rating 60A/5A. It's available but I use CT rating 100A/5A. I's not available. Who can help me and advice me ?
Thank you.
Best regards.